InspectionMethodBuilderScanModeTypes Enumeration

NXOpen.CAM.InspectionMethodBuilder.ScanModeTypes is an alias for NXOpen.CAM.InspectionMethodBuilderScanModeTypes

class NXOpen.CAM.InspectionMethodBuilderScanModeTypes

Bases: object

the scan mode 3-axis, 5-axis type

Enum Members

Enum Member Enum Member Description
Mode3axis
3-axis mode
Mode5axis
5-axis mode
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.