InspectionMethodBuilderSurfaceProfileTypes Enumeration

NXOpen.CAM.InspectionMethodBuilder.SurfaceProfileTypes is an alias for NXOpen.CAM.InspectionMethodBuilderSurfaceProfileTypes

class NXOpen.CAM.InspectionMethodBuilderSurfaceProfileTypes

Bases: object

the analysis surface profile fitting type

Enum Members

Enum Member Enum Member Description
MinimumDeviationNormal
Minimum Deviation - Normal
MinimumDeviation3D
Minimum Deviation - 3D
LeastSquaresNormal
Least Squares - Normal
LeastSquares3D
Least Squares - 3D
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.