InspectionMethodBuilderUVModeTypes Enumeration

NXOpen.CAM.InspectionMethodBuilder.UVModeTypes is an alias for NXOpen.CAM.InspectionMethodBuilderUVModeTypes

class NXOpen.CAM.InspectionMethodBuilderUVModeTypes

Bases: object

the UV modes

Enum Members

Enum Member Enum Member Description
Percentage
Percentage
Distance
Distance from start and end in part units
Full
Full circumference
Degrees
Angle from start and end
Sweep
Start angle and sweep angle
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.