InspectionMoveBuilderSensorStrategyTypes Enumeration

NXOpen.CAM.InspectionMoveBuilder.SensorStrategyTypes is an alias for NXOpen.CAM.InspectionMoveBuilderSensorStrategyTypes

class NXOpen.CAM.InspectionMoveBuilderSensorStrategyTypes

Bases: object

the sensor selection strategy

Enum Members

Enum Member Enum Member Description
CreateAsNeeded
Create as needed
UseExisting
Use existing only
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.