InspectionMoveBuilderProbeTipTypes Enumeration

NXOpen.CAM.InspectionMoveBuilder.ProbeTipTypes is an alias for NXOpen.CAM.InspectionMoveBuilderProbeTipTypes

class NXOpen.CAM.InspectionMoveBuilderProbeTipTypes

Bases: object

the preferred probe tip type

Enum Members

Enum Member Enum Member Description
Any
Any tip type
Sphere
Sphere tip
Cylinder
Cylinder tip
Disk
Disk tip
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.