InspectionMethodBuilderAxisExtrapolationTypes Enumeration

NXOpen.CAM.InspectionMethodBuilder.AxisExtrapolationTypes is an alias for NXOpen.CAM.InspectionMethodBuilderAxisExtrapolationTypes

class NXOpen.CAM.InspectionMethodBuilderAxisExtrapolationTypes

Bases: object

the analysis axis extrapolation type

Enum Members

Enum Member Enum Member Description
On
Extrapolate
Off
Do not extrapolate
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.