ParamBuilder Class¶
-
class
NXOpen.CAM.
ParamBuilder
¶ Bases:
NXOpen.Builder
Represents a manufacturing object builder.
It is the top level builder for all manufacturing objects that have a representation in the Operation Navigator.
This is an abstract class and cannot be instantiated.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
OptimizationMethod | Returns or sets the optim method |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ParamBuilderOptimizationTypes Enumeration | Available types for Optimization Method in operation |
Property Detail¶
CycleEvent¶
-
ParamBuilder.
CycleEvent
¶ Returns the cycle event
-------------------------------------
Getter Method
Signature
CycleEvent()
Returns: the cycle event Return type: NXOpen.CAM.Ude
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
CycleTable¶
-
ParamBuilder.
CycleTable
¶ Returns the cycle
-------------------------------------
Getter Method
Signature
CycleTable()
Returns: the cycle table Return type: NXOpen.CAM.Cycle
New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
OptimizationMethod¶
-
ParamBuilder.
OptimizationMethod
¶ Returns or sets the optim method
-------------------------------------
Getter Method
Signature
OptimizationMethod()
Returns: the optim method Return type: NXOpen.CAM.ParamBuilderOptimizationTypes
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
OptimizationMethod(optimMethod)
Parameters: optimMethod ( NXOpen.CAM.ParamBuilderOptimizationTypes
) – the optim methodNew in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
ParamBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.