InspectionMethodBuilderScanHelixTurnTypes Enumeration

NXOpen.CAM.InspectionMethodBuilder.ScanHelixTurnTypes is an alias for NXOpen.CAM.InspectionMethodBuilderScanHelixTurnTypes

class NXOpen.CAM.InspectionMethodBuilderScanHelixTurnTypes

Bases: object

the helix turn type

Enum Members

Enum Member Enum Member Description
Pitch
Pitch
SweepAngle
Sweep Angle
Revolutions
Revolutions
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.