MethodBuilder Class¶
-
class
NXOpen.CAM.
MethodBuilder
¶ Bases:
NXOpen.CAM.NCGroupBuilder
Represents a Method Builder
This is an abstract class, and cannot be instantiated.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
CutParameters | Returns the cut parameter object |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndUdeSet | Returns the end ude set |
OptimizationMethod | Returns or sets the optim method |
PaintDisplay | Returns the sub builder for paint display |
PathDisplay | Returns the sub builder for path display |
PathDisplayColors | Returns the sub builder for path display colors |
SilhouDisplay | Returns the sub builder for silhou display |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
ToolDisplay | Returns the sub builder for tool display |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCutMethod | Get cut method @return |
GetObject | Returns the object currently being edited by this builder. |
SetCutMethod | Set cut method |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CutParameters¶
-
MethodBuilder.
CutParameters
¶ Returns the cut parameter object
-------------------------------------
Getter Method
Signature
CutParameters()
Returns: Return type: NXOpen.CAM.CutParameters
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
PaintDisplay¶
-
MethodBuilder.
PaintDisplay
¶ Returns the sub builder for paint display
-------------------------------------
Getter Method
Signature
PaintDisplay()
Returns: the paint_display Return type: NXOpen.CAM.DisplayPaint
New in version NX7.5.0.
License requirements: None.
PathDisplay¶
-
MethodBuilder.
PathDisplay
¶ Returns the sub builder for path display
-------------------------------------
Getter Method
Signature
PathDisplay()
Returns: the path_display Return type: NXOpen.CAM.DisplayPath
New in version NX7.5.0.
License requirements: None.
PathDisplayColors¶
-
MethodBuilder.
PathDisplayColors
¶ Returns the sub builder for path display colors
-------------------------------------
Getter Method
Signature
PathDisplayColors()
Returns: the path_display_colors Return type: NXOpen.CAM.PathDisplayColors
New in version NX7.5.0.
License requirements: None.
SilhouDisplay¶
-
MethodBuilder.
SilhouDisplay
¶ Returns the sub builder for silhou display
-------------------------------------
Getter Method
Signature
SilhouDisplay()
Returns: the silhou_display Return type: NXOpen.CAM.DisplaySilhouette
New in version NX7.5.0.
License requirements: None.
ToolDisplay¶
-
MethodBuilder.
ToolDisplay
¶ Returns the sub builder for tool display
-------------------------------------
Getter Method
Signature
ToolDisplay()
Returns: the tool_display Return type: NXOpen.CAM.DisplayTool
New in version NX7.5.0.
License requirements: None.
Method Detail¶
GetCutMethod¶
-
MethodBuilder.
GetCutMethod
¶ Get cut method
Signature
GetCutMethod()
Returns: Return type: str New in version NX8.0.1.
License requirements: None.
SetCutMethod¶
-
MethodBuilder.
SetCutMethod
¶ Set cut method
Signature
SetCutMethod(libRef)
Parameters: libRef (str) – New in version NX8.0.1.
License requirements: cam_base (“CAM BASE”)
Validate¶
-
MethodBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.