DisplayPaint Class¶
-
class
NXOpen.CAM.
DisplayPaint
¶ Bases:
NXOpen.TaggedObject
Represents a display paint Builder
This is an abstract class and cannot be instantiated.
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
ArrowDisplayFlag | Returns or sets the arrow display flag |
FeedDisplayFlag | Returns or sets the feed display flag |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
ArrowDisplayFlag¶
-
DisplayPaint.
ArrowDisplayFlag
¶ Returns or sets the arrow display flag
-------------------------------------
Getter Method
Signature
ArrowDisplayFlag()
Returns: the arrow display flag Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ArrowDisplayFlag(arrowDisplay)
Parameters: arrowDisplay (bool) – the arrow display flag New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
FeedDisplayFlag¶
-
DisplayPaint.
FeedDisplayFlag
¶ Returns or sets the feed display flag
-------------------------------------
Getter Method
Signature
FeedDisplayFlag()
Returns: the feed display flag Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeedDisplayFlag(feedDisplay)
Parameters: feedDisplay (bool) – the feed display flag New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)