InspectionMethodBuilderScanCurveModeTypes Enumeration

NXOpen.CAM.InspectionMethodBuilder.ScanCurveModeTypes is an alias for NXOpen.CAM.InspectionMethodBuilderScanCurveModeTypes

class NXOpen.CAM.InspectionMethodBuilderScanCurveModeTypes

Bases: object

the scan curve mode

Enum Members

Enum Member Enum Member Description
ExistingCurve
Use existing curve
AutoCurve
Autogenerate curves
OffsetCurve
Offset curve
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.