InspectionMethodBuilderScanHelixTurnDirectionTypes Enumeration

NXOpen.CAM.InspectionMethodBuilder.ScanHelixTurnDirectionTypes is an alias for NXOpen.CAM.InspectionMethodBuilderScanHelixTurnDirectionTypes

class NXOpen.CAM.InspectionMethodBuilderScanHelixTurnDirectionTypes

Bases: object

the helix turn direction type

Enum Members

Enum Member Enum Member Description
Right
Right hand turn
Left
Left hand turn
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.