InspectionMethodBuilderInspectionModes Enumeration

NXOpen.CAM.InspectionMethodBuilder.InspectionModes is an alias for NXOpen.CAM.InspectionMethodBuilderInspectionModes

class NXOpen.CAM.InspectionMethodBuilderInspectionModes

Bases: object

CMM Inspection modes.

Enum Members

Enum Member Enum Member Description
ProgramDefault
Program Default
Program
Program
Manual
Manual
Auto
Auto
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.