reset (EventController)
Syntax
<Path>.reset |
The method reset makes the EventController designated by <Path> execute all methods in your simulation model that are named reset. Plant Simulation deletes all unprocessed events, resets the simulation time to 0, resets the statistics, clears all failures of all objects, and sets all objects to the state planned.
Note that the request control, the receive control, and the release control of the Importer are not called when you reset the simulation.
Plant Simulation does not execute the Reset immediately, but only when all methods being executed at the moment have been executed all the way. This includes the method, which has triggered the Reset. The methods init and start behave like this as well.
Example
EventController.reset |
Related Topics
Reset Simulation button in the EventController
Reset Simulation button in the EventDebugger
reset, method in SimTalk
Related Topics
Methods of the EventControllergetBreakpointCondition
getBreakpointReceiver
getBreakpointSender
getBreakpointStartTime
getBreakpointStopTime
getBreakpointTraceFile
getBreakpointType
getEventList
init (EventController)
setBreakpointCondition
setBreakpointReceiver
setBreakpointSender
setBreakpointStartTime
setBreakpointStopTime
setBreakpointTraceFile
setBreakpointType
start (EventController)
startWithoutAnimation
stop (EventController)