setBreakpointStartTime
Syntax
<Path>.setBreakpointStartTime(LineInBreakpointList:integer, StartTime:time or dateTime) → time |
The method setBreakpointStartTime sets the Start time at which the breakpoint of the breakpoint of the EventController designated by <Path> will be activated.
Parameters
The parameter LineInBreakpointList of data type integer designates the line of the breakpoint in the breakpoint list.
The parameter StartTime of data type time designates the time at which the breakpoint will be activated.
Return Value
The return value has the data type time.
Example
print EventController.setBreakpointStartTime(2,15) |
Related Topic
Related Topics
Methods of the EventControllergetBreakpointCondition
getBreakpointReceiver
getBreakpointSender
getBreakpointStartTime
getBreakpointStopTime
getBreakpointTraceFile
getBreakpointType
getEventList
init (EventController)
reset (EventController)
setBreakpointCondition
setBreakpointReceiver
setBreakpointSender
setBreakpointStopTime
setBreakpointTraceFile
setBreakpointType
start (EventController)
startWithoutAnimation
stop (EventController)