getEventList
Syntax
<Path>.getEventList(MaximumNumberOfEvents:integer) → table |
The method getEventList returns the List of scheduled events of the EventController designated by <Path>.
Parameter
The parameter MaximumNumberOfEvents of data type integer designates the maximum number of events, which the EventController writes to the data table.
Enter getEventList(-1) to write all events to the data table. The event list provides the columns Type, Time, Receiver, Sender, Insertion Time, and Parameters.
Return Value
The return value has the data type table.
Example
TableVariable := EventController.getEventList(-1) |
Related Topics
Methods of the EventControllergetBreakpointCondition
getBreakpointReceiver
getBreakpointSender
getBreakpointStartTime
getBreakpointStopTime
getBreakpointTraceFile
getBreakpointType
init (EventController)
reset (EventController)
setBreakpointCondition
setBreakpointReceiver
setBreakpointSender
setBreakpointStartTime
setBreakpointStopTime
setBreakpointTraceFile
setBreakpointType
start (EventController)
startWithoutAnimation
stop (EventController)