setBreakpointReceiver
Syntax
<Path>.setBreakpointReceiver(LineInBreakpointList:integer, ReceivingObject:object) → object |
The method setBreakpointReceiver sets the Receiver of the breakpoint of the EventController designated by <Path>.
Parameters
The parameter LineInBreakpointList of data type integer designates the line of the breakpoint in the breakpoint list.
The parameter ReceivingObject of data type object designates the object that receives the breakpoint.
Return Value
The return value has the data type object.
Example
print EventController.setBreakpointReceiver(2,drain) |
Related Topic
Related Topics
Methods of the EventControllergetBreakpointCondition
getBreakpointReceiver
getBreakpointSender
getBreakpointStartTime
getBreakpointStopTime
getBreakpointTraceFile
getBreakpointType
getEventList
init (EventController)
reset (EventController)
setBreakpointCondition
setBreakpointSender
setBreakpointStartTime
setBreakpointStopTime
setBreakpointTraceFile
setBreakpointType
start (EventController)
startWithoutAnimation
stop (EventController)