setBreakpointType
Syntax
<Path>.setBreakpointType(LineInBreakpointList:integer, EventType:string) → string |
The method setBreakpointType sets the type of Type of event for which the breakpoint of the EventController designated by <Path> is active.
Parameters
The parameter LineInBreakpointList of data type integer designates the line of the breakpoint in the breakpoint list.
The parameter EventType of data type string designates the type of event for which the breakpoint will be active.
Return Value
The return value has the data type string.
Example
print EventController.setBreakpointType(2,"Pause") |
Related Topic
Related Topics
Methods of the EventControllergetBreakpointCondition
getBreakpointReceiver
getBreakpointSender
getBreakpointStartTime
getBreakpointStopTime
getBreakpointTraceFile
getBreakpointType
getEventList
init (EventController)
reset (EventController)
setBreakpointCondition
setBreakpointReceiver
setBreakpointSender
setBreakpointStartTime
setBreakpointStopTime
setBreakpointTraceFile
start (EventController)
startWithoutAnimation
stop (EventController)