getBreakpointReceiver
Syntax
<Path>.getBreakpointReceiver(LineInBreakpointList:integer) → object |
The method getBreakpointReceiver returns the object that receives the breakpoint of the EventController designated by <Path>, i.e., the Receiver.
Parameter
The parameter LineInBreakpointList of data type integer designates the line of the breakpoint in the breakpoint list.
Return Value
The return value has the data type object.
Example
print EventController.getBreakpointReceiver(1) |
Related Topic
Related Topics
Methods of the EventControllergetBreakpointCondition
getBreakpointSender
getBreakpointStartTime
getBreakpointStopTime
getBreakpointTraceFile
getBreakpointType
getEventList
init (EventController)
reset (EventController)
setBreakpointCondition
setBreakpointReceiver
setBreakpointSender
setBreakpointStartTime
setBreakpointStopTime
setBreakpointTraceFile
setBreakpointType
start (EventController)
startWithoutAnimation
stop (EventController)