setBreakpointTraceFile
Syntax
<Path>.setBreakpointTraceFile(LineInBreakpointList:integer, FileName:string) → string |
The method setBreakpointTraceFile the name of the Trace file into which the EventController designated by <Path> writes the events.
Parameters
The parameter LineInBreakpointList of data type integer designates the line of the breakpoint in the breakpoint list.
The parameter FileName of data type string designates the name of the trace file.
Return Value
The return value has the data type string.
Example
print EventController.setBreakpointTraceFile(2, "C:\users\hawthorne\myTracefile.txt") |
Related Topic
Related Topics
Methods of the EventControllergetBreakpointCondition
getBreakpointReceiver
getBreakpointSender
getBreakpointStartTime
getBreakpointStopTime
getBreakpointTraceFile
getBreakpointType
getEventList
init (EventController)
reset (EventController)
setBreakpointCondition
setBreakpointReceiver
setBreakpointSender
setBreakpointStartTime
setBreakpointStopTime
setBreakpointType
start (EventController)
startWithoutAnimation
stop (EventController)