getBreakpointTraceFile
Syntax
<Path>.getBreakpointTraceFile(LineInBreakpointList:integer) → string |
The method getBreakpointTraceFile returns the name of the Trace file to which of the EventController designated by <Path> writes the events.
Parameter
The parameter LineInBreakpointList of data type integer designates the line of the breakpoint in the breakpoint list.
Return Value
The return value has the data type string.
Example
print EventController.getBreakpointTraceFile(4) |
Related Topic
Related Topics
Methods of the EventControllergetBreakpointCondition
getBreakpointReceiver
getBreakpointSender
getBreakpointStartTime
getBreakpointStopTime
getBreakpointType
getEventList
init (EventController)
reset (EventController)
setBreakpointCondition
setBreakpointReceiver
setBreakpointSender
setBreakpointStartTime
setBreakpointStopTime
setBreakpointTraceFile
setBreakpointType
start (EventController)
startWithoutAnimation
stop (EventController)