getBreakpointSender
Syntax
<Path>.getBreakpointSender(ConveyorInBreakpointList:integer) → object |
The method getBreakpointSender returns the object that sends the breakpoint, of the EventController designated by <Path>, i.e., the Sender.
Parameter
The parameter ConveyorInBreakpointList of data type integer designates the row of the breakpoint in the breakpoint list.
Return Value
The return value has the data type object.
Example
print EventController.getBreakpointSender(3) |
Related Topic
Related Topics
Methods of the EventControllergetBreakpointCondition
getBreakpointReceiver
getBreakpointStartTime
getBreakpointStopTime
getBreakpointTraceFile
getBreakpointType
getEventList
init (EventController)
reset (EventController)
setBreakpointCondition
setBreakpointReceiver
setBreakpointSender
setBreakpointStartTime
setBreakpointStopTime
setBreakpointTraceFile
setBreakpointType
start (EventController)
startWithoutAnimation
stop (EventController)