Methods of the EventController
The EventController provides:
The methods getBreakpointCondition, getBreakpointReceiver, getBreakpointSender, getBreakpointStartTime, getBreakpointStopTime, getBreakpointTraceFile, getBreakpointType, getEventList, init, reset, setBreakpointCondition, setBreakpointReceiver, setBreakpointSender, setBreakpointStartTime, setBreakpointStopTime, setBreakpointTraceFile, setBreakpointType, start, startWithoutAnimation, and stop.
To view all of the methods and attributes of the EventController, open the window Show Attributes and Methods. The figure below illustrates the information using the example of the object Source.
Select Show Attributes and Methods on the context menu of the Class Library to show the attributes and methods of the selected Class.
Press the F8 key or click Show Attributes and Methods on the Home ribbon tab of the Frame into which you inserted an instance to show the attributes and methods of the selected Instance.
An example of the Syntax line of the individual methods might look like this:
<Path>.derive(Destination:object, Name:string) → object |
The expression Path designates the path of the object to which the method applies.
The signature of the method, consisting of the identifier and the data type of the parameter, is listed in parentheses. The expression (Parameter:string), for example, designates a parameter of data type string. Instead of a constant value, you can also use a variable of the required type or a method that returns the required data type.
Optional parameters are listed within square brackets. The expression [,Parameter:boolean], for example, means that you can, but do not have to enter the boolean parameter.
Note:Make sure to enter the parentheses for expressions within parentheses (…). Not entering them may lead to unexpected results and open the Debugger.
Related Topics
getBreakpointConditiongetBreakpointReceiver
getBreakpointSender
getBreakpointStartTime
getBreakpointStopTime
getBreakpointTraceFile
getBreakpointType
getEventList
init (EventController)
reset (EventController)
setBreakpointCondition
setBreakpointReceiver
setBreakpointSender
setBreakpointStartTime
setBreakpointStopTime
setBreakpointTraceFile
setBreakpointType
start (EventController)
startWithoutAnimation
stop (EventController)