getBreakpointStartTime
Syntax
<Path>.getBreakpointStartTime(LineInBreakpointList:integer) → time |
The method getBreakpointStartTime returns the time at which the breakpoint becomes active of the EventController designated by <Path>, i.e., the Start time.
Parameter
The parameter LineInBreakpointList of data type integer designates the line of the breakpoint in the breakpoint list.
Return Value
The return value has the data type time.
Example
print EventController.getBreakpointStartTime(5) |
Related Topic
Related Topics
Methods of the EventControllergetBreakpointCondition
getBreakpointReceiver
getBreakpointSender
getBreakpointStopTime
getBreakpointTraceFile
getBreakpointType
getEventList
init (EventController)
reset (EventController)
setBreakpointCondition
setBreakpointReceiver
setBreakpointSender
setBreakpointStartTime
setBreakpointStopTime
setBreakpointTraceFile
setBreakpointType
start (EventController)
startWithoutAnimation
stop (EventController)