stop (EventController)
Syntax
<Path>.stop[(EndSim:boolean := false]) |
The method stop stops the EventController and terminates the simulation run.
Parameter
The optional parameter EndSim of data type boolean set if the simulation will be stopped and if the endSim methods will be executed (true) or if the simulation will only be stopped (false).
The default value is false.
Example
root.EventController.stop |
Related Topic
Related Topics
Methods of the EventControllergetBreakpointCondition
getBreakpointReceiver
getBreakpointSender
getBreakpointStartTime
getBreakpointStopTime
getBreakpointTraceFile
getBreakpointType
getEventList
init (EventController)
reset (EventController)
setBreakpointCondition
setBreakpointReceiver
setBreakpointSender
setBreakpointStartTime
setBreakpointStopTime
setBreakpointTraceFile
setBreakpointType
start (EventController)
startWithoutAnimation