Start/Stop Simulation (EventController)
To start the simulation, click . To stop the simulation after the active simulation event has been processed, click the button again. The program calls init methods when you click Start/Stop Simulation if they have not been called yet.
Instead, you can also click on the Home Ribbon Tab or double-click the icon of the EventController while holding the Shift key down.
Or you can right-click the EventController in the Frame and select Start/Stop Simulation on the context menu.
SimTalk:
init,
Related Topics
Init control of the EventController
Init control of the Transporter