InitCtrl (EventController)
Syntax
<Path>.InitCtrl:method |
The attribute InitCtrl designates a Method object. Plant Simulation calls this control once at the beginning of the simulation run during the init phase before the objects are initialized and before init methods are executed.
Data Type of the Value You Can Assign
You can assign a value of data type method.
Example
EventController.InitCtrl := &myInitControl |
-- The source code of an init control might look like this: |
Related Topics
Define How Many Workers Are Created When the Model is Initialized
Related Topics
Attributes of the EventControllerAbsTimeFormat
BreakPointsActive
Date (EventController)
DeleteMUsOnReset
End (EventController)
ExperimentManager
IncrementRandomNumbersVariantOnReset
RandomNumbersVariant
RealTime
RealTimeScale
ResetCtrl
Speed (EventController)
StartStat
StartStopCtrl
SummaryReport
TraceActive
TraceFile