RealTime
Syntax
<Path>.RealTime:boolean |
The attribute RealTime sets if the EventController will wait for the time span between events during the simulation to elapse in real-time (true) or not (false).
Note:
Activate real-time mode to achieve a smooth 3D-animation. Imported animations only run in this mode.
Data Type of the Value You Can Assign
You can assign a value of data type boolean.
Example
EventController.RealTime := false |
Related Topic
Related Topics
Attributes of the EventControllerAbsTimeFormat
BreakPointsActive
Date (EventController)
DeleteMUsOnReset
End (EventController)
ExperimentManager
IncrementRandomNumbersVariantOnReset
InitCtrl (EventController)
RandomNumbersVariant
RealTimeScale
ResetCtrl
Speed (EventController)
StartStat
StartStopCtrl
SummaryReport
TraceActive
TraceFile