ResetCtrl
Syntax
<Path>.ResetCtrl:object |
The attribute ResetCtrl designates a Method object, which is called, whenever you click Reset Simulation in the EventController or when the method reset is called. Note that Plant Simulation calls this control before calling any reset method you inserted in the Frame and any of its sub-Frames.
Data Type of the Value You Can Assign
You can assign a value of data type object.
Example
EventController.ResetCtrl := &myResetMethod |
Related Topics
Reset Simulation button in the EventController
Reset Simulation button in the EventDebugger
reset method
Related Topics
Attributes of the EventControllerAbsTimeFormat
BreakPointsActive
Date (EventController)
DeleteMUsOnReset
End (EventController)
ExperimentManager
IncrementRandomNumbersVariantOnReset
InitCtrl (EventController)
RandomNumbersVariant
RealTime
RealTimeScale
Speed (EventController)
StartStat
StartStopCtrl
SummaryReport
TraceActive
TraceFile