RealTimeScale
Syntax
<Path>.RealTimeScale:real |
The attribute RealTimeScale sets the time factor that elapses between two events in real-time. The duration of an event in real-time is the simulation time divided by the scaling factor you enter. The resulting duration is an integer.
Data Type of the Value You Can Assign
You can assign a value of data type real.
Example
EventController.RealTimeScale := 10 |
Related Topic
Related Topics
Attributes of the EventControllerAbsTimeFormat
BreakPointsActive
Date (EventController)
DeleteMUsOnReset
End (EventController)
ExperimentManager
IncrementRandomNumbersVariantOnReset
InitCtrl (EventController)
RandomNumbersVariant
RealTime
ResetCtrl
Speed (EventController)
StartStat
StartStopCtrl
SummaryReport
TraceActive
TraceFile