StartStopCtrl
Syntax
<Path>.StartStopCtrl:method |
The attribute StartStopCtrl designates a Method object, which is called, whenever you click Start/Stop Simulation in the EventController. Note that, whenever you click Single Step Simulation in the EventController, Plant Simulation calls the method, processes the next event, and calls the method again.
Data Type of the Value You Can Assign
You can assign a value of data type method.
You can use the expression ?.IsRunning in the code of the control to tell if the EventController was started (false) or stopped (true).
Example
EventController.StartStopCtrl := &myStartStopControl |
Related Topic
Related Topics
Attributes of the EventControllerAbsTimeFormat
BreakPointsActive
Date (EventController)
DeleteMUsOnReset
End (EventController)
ExperimentManager
IncrementRandomNumbersVariantOnReset
InitCtrl (EventController)
RandomNumbersVariant
RealTime
RealTimeScale
ResetCtrl
Speed (EventController)
StartStat
SummaryReport
TraceActive
TraceFile