List
To open the Dialog Window of the Event Debugger, click this.
The event list contains the types of scheduled events, which the objects in your simulation model entered and which the EventController has to process. It is sorted ascending by time. It lists the type of event, the scheduled processing time, the receiver and the sender of the event, and parameters.
The column Breakpoint shows an S, for a breakpoint which you inserted by double-clicking a cell in the row.
Double-click a cell in the row where you would like to insert a single breakpoint. Then the Event Debugger stops the simulation immediately before the EventController processes that event. Double-click again to remove the breakpoint.
The column Type shows the type of the event.
The column Time shows the point in time at which the event is going to be executed.
The column Receiver shows the object that receives the simulation event.
The column Sender shows the object that sends the simulation event.
The column Insertion Time shows the point in time at which the event was entered into the event list. This column is hidden by default. Drag the column separator to show it.
The column Parameters shows additional information for certain event types, for example the sensor ID (SensorStart), the name of the failure profile (DisruptionBegin), or the parameters passed to a Method (MethCall).
Plant Simulation provides these simulation events:
Event English | Event German | Action taking place/state of the object |
---|---|---|
* | * | stands for any type of event |
Animation | Animation | shows an MU on a Track, Conveyor, and on a Buffer |
Battery | Batterie | the battery of a Transporter is full, empty or on reserve |
BlockageEnd | BlockierEnde | the MU is unblocked |
Bump | Anstoss | the Transporter collides with another MU |
CheckMUDistance | BEAbstandPrüfen | the Conveyor checks if you entered the desiredMU distance between the parts it transports |
CreateMU | ErzeugeBE | the Source object attempts to create MUs |
DeliverParts | TeileAbliefern | the Worker picks up parts at a station and carries them to the target object |
DestroyMU | VernichteBE | the MU is removed from the model |
DisruptionBegin | StörBeginn | the failure of the object begins |
DisruptionEnd | StörEnde | the failure of the object ends |
Distance | Abstand | the Distance control of the Transporter is called |
EndOfTime | ZeitBeendet | the PickAndPlaceRobot is done loading/unloading the Worker is done loading/unloading the Mixer has finished mixing products Converter/AngularConverter is done changing the conveying direction of the MU |
EndOfTurn | EndeDrehen | the PickAndPlaceRobot, Turnplate, Turntable reaches the end position of the rotation |
EndSim | EndSim | terminates the simulation after Plant Simulation has processed all events |
EntranceEnd | EintrittEnde | the rear of the MU entered a length-oriented object the denoted amount of a educt of the Mixer has been reached the MU of the Portioner has been filled all the way the Worker has reached its target station when he is moving freely within the area |
FinalSpeed | EndGeschw | point in time at which the Transporter or the Conveyor reach their final speed after acceleration or deceleration |
GenDuration | GenDauer | activates the duration control of a Generator |
GenInterval | GenAbstand | activates the interval control of a Generator |
Init | Init | initializes the simulation model using the method Init before executing the next scheduled event |
InitStat | InitStat | resets statistics and starts collecting statistics anew |
MethCall | MethAufr | Plant Simulation calls a method that was scheduled with the SimTalk method methCall of the object Method |
MethWakeup | MethAufwecken | continue executing the call chain after the time you entered in a wait statement has elapsed |
Out | Aus | an MU exits the object |
OutEnd | AusEnde | the rear of the MU exits a length-oriented object (Conveyor, Turntable, Track, TwoLaneTrack ) |
Pause | Pause | the object is paused. This event will only be created when you paused the object with the method pauseIn |
PauseEnd | PauseEnde | the object is unpaused. This event will only be created when you paused the object with the method pause |
PositionReached | PositionErreicht | the MU has reached the center of rotation of Turnplate/Turntable the AngularConverter/Converter has reached the point at which the conveying direction changes the Transporter has reached the target |
PoweringUpDown | HochRunterfahren | the material flow object powers up or down to reflect a change in its energy status |
Reference | Referenz | the booking point of the MU exits the object |
SensorBookPos | SensorBuchPos | a sensor is activated by the booking point of the MU |
SensorEnd | SensorEnde | a sensor is activated by the rear of the MU |
SensorStart | SensorBeginn | a sensor is activated by the front of the MU |
SetupEnd | RuestenEnde | the set-up time of an MU has expired |
Shift | Schicht | schedules the beginning or the end of the next shift |
ShiftCalendarStart | SchichtkalenderStart | sets the state of the objects controlled by the ShiftCalendar according to the state it controls |
StartActions | StarteAktionen | determines if the entrance control of the object is activated before starting the actions that are performed when a part enters the object the FluidSource starts producing the fluid new material begins to flow into the Mixer after it ran dry |
StartTransporter | FahrzeugStarten | sets the time after which a Transporter, which collided with the one driving in front of it, starts moving after the first Transporter started again |
TankEmpty | TankLeer | the Tank is empty the MU of the Portioner has been emptied the mixing container of the Mixer is empty |
TankFull | TankVoll | the Tank is full the mixing container of the Mixer is full |
TimeSequence | Zeitleiste | the TimeSequence registers data |
TriggerAction | TriggerAktion | the values of the Trigger changes |
TriggerStart | TriggerStart | the active time of the Trigger starts |
TurnAnimation | DrehAnimation | animates the rotation of PickAndPlaceRobot/Turnplate/Turntable |
UpdateDisplay | UpdateDisplay | updates the values of the object Display |
ZeroSpeed | NullGeschw | point in time when the Transporter or the Conveyor reach the speed 0 after decelerating |
SimTalk:
Related Topics