GetDisruptionEndTime
Syntax
<Path>.GetDisruptionEndTime → time |
The read-only attribute GetDisruptionEndTime returns the point in time at which the next end of a failure (compare DisruptionEnd in the list of scheduled events) is scheduled to take place.
The read-only attribute GetDisruptionEndTime only considers automatically created events. The read-only attribute does not consider a failure event which you manually inserted with the methods startFailure or startFailureIn.
Return Value
The return value has the data type time.
If no event exists, the method returns -1.
Example
print mystation.GetDisruptionEndTime |
Related Topic
Related Topics
Read-Only Attributes for the State of the Material Flow ObjectsFull (material flow objects)
GetDisruptionBeginTime
Occupied (material flow objects)
Operational
Ready (material flow objects)
ResBlocked (material flow objects)
ResCurrentState (material flow objects)
ResSetUp (material flow objects)
ResWaiting (material flow objects)
ResWorking (material flow objects)
TimeUntilEntranceOpen (material flow objects)