GetDisruptionBeginTime
Syntax
<Path>.GetDisruptionBeginTime → time |
The read-only attribute GetDisruptionBeginTime returns the point in time at which the next start of a failure (compare DisruptionBegin in the list of scheduled events) is scheduled to take place.
The read-only attribute GetDisruptionBeginTime only considers automatically created events. The read-only attribute does not consider a failure event which manually you inserted with the methods startFailure or startFailureIn.
Return Value
The return value has the data type time.
If no event exists, the method returns -1.
Example
print mystation.GetDisruptionBeginTime |
Related Topic
Related Topics
Read-Only Attributes for the State of the Material Flow ObjectsFull (material flow objects)
GetDisruptionEndTime
Occupied (material flow objects)
Operational
Ready (material flow objects)
ResBlocked (material flow objects)
ResCurrentState (material flow objects)
ResSetUp (material flow objects)
ResWaiting (material flow objects)
ResWorking (material flow objects)
TimeUntilEntranceOpen (material flow objects)