ResSetUp (material flow objects)
Syntax
<Path>.ResSetUp → boolean |
The read-only attribute ResSetUp returns if the object designated by <Path> is Setting-Up and not failed, not paused, or not stopped (true) or not (false).
Return Value
The return value has the data type boolean.
Example
if machA.ResSetUp |
Related Topics
Related Topics
Read-Only Attributes for the State of the Material Flow ObjectsFull (material flow objects)
GetDisruptionEndTime
GetDisruptionBeginTime
Occupied (material flow objects)
Operational
Ready (material flow objects)
ResBlocked (material flow objects)
ResCurrentState (material flow objects)
ResWaiting (material flow objects)
ResWorking (material flow objects)
TimeUntilEntranceOpen (material flow objects)