Interface | Description |
---|---|
AddObjectsToRegionBuilder |
Creates the builder for associating the symbols from library to the region
To create a new instance of this class, use DrawingRegionCollection.createAddObjectsToRegionBuilder() Created in NX8.0.0 |
AddRemoveBoxViewBuilder |
This class is used to construct the add remove box view Builder
To create a new instance of this class, use DraftingViewCollection.createAddRemoveBoxViewBuilder(nxopen.drawings.DraftingView) Created in NX8.0.0 |
AnnotationSettingsBuilder |
Represents a
Drawings.AnnotationSettingsBuilder . |
AutomationBookletBuilder | |
AutomationTemplateRegionBuilder | |
BaseHalfSectionLine |
Represents a Base Half Section Line.
|
BasePointToPointSectionLine |
Represents a Base Point to Point Section Line.
|
BaseSteppedSectionLine |
Represents a Base Stepped Section Line.
|
BaseView |
Represents a Base View.
|
BaseViewBuilder |
Represents a
BaseView builder To create a new instance of this class, use DraftingViewCollection.createBaseViewBuilder(nxopen.drawings.BaseView) Default values. |
BaseViewStyle |
Represents set of Base View Style Preferences applicable to drafting views.
|
BorderAndZoneStyleBuilder |
Represents the Border and Zone Style Builder which manages all the style attributes related
to sheet borders, sheet margins and sheet zones.
|
BordersAndZones |
Represents Borders and Zones
To create or edit an instance of this class, use BordersAndZonesBuilder Created in NX8.0.0 |
BordersAndZonesBuilder |
Builder for creating Borders and Zones.
|
BordersAndZonesCollection |
Represents a collection of
BordersAndZones objects To obtain an instance of this class, refer to DraftingManager Created in NX8.0.0 |
BrokenViewBuilder |
This class is used to construct the broken view Builder
To create a new instance of this class, use DraftingViewCollection.createBrokenViewBuilder(nxopen.drawings.ViewBreak) Default values. |
CompareReportBuilder |
Represents a
CompareReportBuilder builder To create a new instance of this class, use DrawingCompareManager.createCompareReportBuilder() Created in NX7.5.0 |
ConversionProcessSettingsBuilder |
Represents a
Drawings.ConversionProcessSettingsBuilder . |
ConvertDraftingContentsBuilder |
Represents a
Drawings.ConvertDraftingContentsBuilder . |
ConvertToPMIBuilderManager |
Represents
ConvertToPMIBuilderManager
To obtain an instance of this class, refer to BasePart Created in NX11.0.0 |
CustomViewSettingsBuilder |
this class represents the "this class represents Drawings.CustomViewSettingsBuilder.
|
DetailView |
Represents a Detail View.
|
DetailViewBuilder |
Represents a
DetailView . |
DraftingBody |
Represents a drafting body.
|
DraftingBodyCollection |
Represents a collection of
DraftingBody s. |
DraftingComponentSelectionBuilder |
This builder allows the user to select a view in which
component objects can be designated as primary or secondary geometry .
|
DraftingCurve |
Represents a Drafting VD Curve.
|
DraftingCurveCollection |
Represents a collection of
DraftingCurve s. |
DraftingCurveInfo |
Represents Drafting Curve Info .
|
DraftingView |
Represents a drafting view.
|
DraftingViewCollection |
Represents a collection of
DraftingView s. |
DrawingCompareSettingsBuilder | Deprecated
Deprecated in NX11.0.0.
|
DrawingFormatSheetBuilder | |
DrawingRegion |
Represents a Drawing Region
To create or edit an instance of this class, use DrawingRegionBuilder Created in NX8.0.0 |
DrawingRegionBuilder |
Represents a Drawing Region Builder
To create a new instance of this class, use DrawingRegionCollection.createDrawingRegionBuilder(nxopen.drawings.DrawingRegion) Default values. |
DrawingRegionCollection |
Represents a collection of drawing regions
Use nxopen.Drawings#drawingRegion to get the instance of this class. |
DrawingRegionRulesBuilder |
Represents a Drawing region rules builder .
|
DrawingSheet |
Represents a drawing sheet.
|
DrawingSheetBuilder |
Represents a
DrawingSheetBuilder
To create a new instance of this class, use DrawingSheetCollection.drawingSheetBuilder(nxopen.drawings.DrawingSheet) Created in NX5.0.0 |
DrawingSheetCollection |
Represents a collection of drawing sheets.
|
DrawingsPropertiesBuilder |
Represents an
DrawingsPropertiesBuilder to be used for marking the
component as secondary geometry. |
DrawingView |
Drawing View - an empty view created without any geometric objects.
|
DrawingViewBuilder |
This builder allows the user to create a Drawing View
To create a new instance of this class, use DraftingViewCollection.createDrawingViewBuilder(nxopen.drawings.DrawingView) Default values. |
EditSectionLineSettingsBuilder |
Represents a
EditSectionLineSettingsBuilder builder. |
EditViewLabelSettingsBuilder |
Represents a
EditViewLabelSettingsBuilder builder. |
EditViewSettingsBuilder |
Represents a
EditViewSettingsBuilder builder. |
FlatPatternObject |
Provides an interface to the data available for flat pattern objects on drawing
views.
|
FlatPatternViewStyle |
Provides access to object and callout properties for sheet-metal data in
flat pattern views on drawings.
|
GeneralViewStyle |
Represents set of General View Styles Preferences applicable to drafting views.
|
GeneralWorkFlowBuilder | |
HalfPictorialSectionLine |
Half Pictorial Section Line is used to create a pictorial view with
half of the part sectioned and the other half un-sectioned.
|
HalfSectionLine |
Half Section Line is used to create a view with half of the part
sectioned and the other half un-sectioned.
|
HalfSectionLineBuilder | Deprecated
Deprecated in NX10.0.0.
|
HiddenLinesViewStyle |
Represents set of Hidden Lines View Style Preferences applicable to drafting views.
|
HiddenObjectsBuilder |
This builder allows the user to select a view in which
component objects can be designated as hidden or shown .
|
HingeLineBuilder |
Represents a Drawings.HingeLineBuilder.
|
InheritPmiViewStyle |
Represents set of InheritPmiViewStyle applicable to drafting views.
|
MarkAsTemplateBuilder |
Represents a
MarkAsTemplateBuilder
To create a new instance of this class, use DraftingManager.createMarkAsTemplateBuilder() Created in NX8.0.0 |
MultipleViewPlacementBuilder |
This builder allows the user to create a Multiple View Placement .
|
OrderManager |
Represents an object that manages orders.
|
OrientationViewStyle |
Represents set of Orientation View Style Preferences applicable to drafting views.
|
OrientedSectionLine |
Represents a Oriented Section Line.
|
OrientedSectionLineBuilder | Deprecated
Deprecated in NX10.0.0.
|
OvtBuilder | |
ParentViewBuilder |
Represents a
ParentViewBuilder . |
PerspectiveViewStyle |
Represents set of PerspectiveViewStyle applicable to drafting views.
|
PictorialSectionLine |
A Pictorial Simple or Pictorial Stepped Section Line.
|
PointAndAngleSectionLine |
Point and Angle Section Line lets you create a view with multiple
segment cuts with no bends.
|
PointAndAngleSectionLineBuilder | Deprecated
Deprecated in NX10.0.0.
|
PointToPointSectionLine |
Point to Point Section Line lets you create a view with multiple
segment cuts with no bends.
|
PointToPointSectionLineBuilder | Deprecated
Deprecated in NX10.0.0.
|
ProjectedView |
Represents a Projected View.
|
ProjectedViewBuilder |
Represents a
ProjectedView builder To create a new instance of this class, use DraftingViewCollection.createProjectedViewBuilder(nxopen.drawings.ProjectedView) Default values. |
ProjectedViewOrientationBuilder | |
ProjectedViewStyle |
Represents set of Projected View Style Preferences applicable to drafting views.
|
RefineDisplayBuilder |
Represents a
RefineDisplayBuilder . |
RemoveObjectsBuilder |
Creates the builder for removing associated objects from the region
To create a new instance of this class, use DrawingRegionCollection.createRemoveObjectsBuilder() Created in NX8.0.0 |
RenderSet |
Represents a RenderSet.
|
ReportBuilder |
Represents a
Drawings.ReportBuilder . |
RevolvedSectionLine |
Revolved Section Line is used to create section views which are
revolved about an axis.
|
RevolvedSectionLineBuilder | Deprecated
Deprecated in NX10.0.0.
|
SecondaryGeometryInViewsBuilder |
This builder allows the user to select existing view(s) in which
component objects can be designated as secondary or primary
To create a new instance of this class, use DraftingViewCollection.createSecondaryGeometryInViewsBuilder() Default values. |
SectionInViewBuilder |
This builder allows the user to select a view in which component or
solid body objects can be designated as section, non-sectioned, or neither
To create a new instance of this class, use DraftingViewCollection.createSectionInViewBuilder() Default values. |
SectionLine |
Represents a Section Line.
|
SectionLineBuilder | Deprecated
Deprecated in NX10.0.0.
|
SectionLineCollection |
Represents a collection of
SectionLine s. |
SectionLineSegmentBuilder |
Represents a
SectionLineSegmentBuilder . |
SectionLineSegmentBuilderList |
Represents a list of objects.
|
SectionLineSegmentPointBuilder |
Represents Section Line Segment Point Builder
To create a new instance of this class, use SectionLineSegmentPointListBuilder.createSectionLineSegmentPointBuilder() Created in NX10.0.0 |
SectionLineSegmentPointListBuilder |
Represents SectionLineSegmentPointListBuilder class.
|
SectionLineSegmentsBuilder |
Represents a class Drawings.SectionLineSegmentsBuilder.
|
SectionLineSettingsBuilder |
Represents the Section Line Settings Builder (Drawings.SectionLineSettingsBuilder) which manages all the style attributes related
to the section Line including label letter.
|
SectionLineStyleBuilder |
Represents a Drawings.SectionLineStyleBuiler.
|
SectionView |
Represents a Section View.
|
SectionViewBuilder |
Represents a
SectionView builder To create a new instance of this class, use DraftingViewCollection.createSectionViewBuilder(nxopen.NXObject) Default values. |
SectionViewStyle |
Represents set of Section View Style Preferences applicable to drafting views.
|
SelectDraftingView |
Represents a single object selection.
|
SelectDraftingViewList |
Represents a list of objects on a selection list.
|
SelectDrawingRegion |
Represents a single object selection.
|
SelectDrawingView |
Represents a single object selection.
|
SelectDrawingViewList |
Represents a list of objects on a selection list.
|
SelectModelViewBuilder |
Represents a Select Model View builder that selects a model view
.
|
SelectRegionBuilder |
Creates the builder for associating the objects from the screen
To create a new instance of this class, use DrawingRegionCollection.createSelectRegionBuilder() Created in NX8.0.0 |
SelectSectionLine |
Represents a single object selection.
|
SettingsBuilder |
Represents a
Drawings.SettingsBuilder . |
ShadingViewStyle |
Represents set of Shading View style applicable to drafting views.
|
SheetBorderSettingsBuilder |
Represents a
SheetBorderSettingsBuilder . |
SheetDraftingViewCollection |
Represents a collection of
DraftingView s. |
SheetMarginSettingsBuilder |
Represents the Drawing Sheet Margins Style Builder.
|
SheetSectionLineCollection |
Represents a collection of
SectionLine s. |
SheetTemplateManager |
Represents a manager of
DraftingView s. |
SheetZoneReferenceBuilder |
builder for creating sheet zone refernce control strings based on the selected attribute and view
To create a new instance of this class, use DraftingManager.createSheetZoneReferenceBuilder() Created in NX8.0.0 |
SheetZoneSettingsBuilder |
Represents the Drawing Sheet Zone Setting Style Builder.
|
ShipbuildingLinesViewStyle |
Represents set of Shipbuilding Lines View Style applicable to drafting views.
|
ShipDraftingViewLinesBuilder |
Represents a ship view lines block
To create a new instance of this class, use DraftingViewCollection.createShipDraftingViewLinesBuilder() Created in NX10.0.0 |
ShipDraftingViewLinesBuilderList |
Represents a list of objects.
|
ShipDraftingViewLinesViewStyle |
Represents set of Ship Drafting Lines View Style applicable to drafting views.
|
SketchedHalfSectionLine |
Sketched Half Section Line is sketch based section line.
|
SketchedPointToPointSectionLine |
Sketched Point to Point Section Line is sketch based section line.
|
SketchedSteppedSectionLine |
A Sketched Simple or Stepped Section Line is sketch based section line.
|
SketchSectionLineBuilder |
Represents a
Drawings.SectionLine builder To create a new instance of this class, use SectionLineCollection.createSketchSectionLineBuilder(nxopen.drawings.SectionLine) Default values. |
SmoothEdgesViewStyle |
Represents set of Smooth Edges View Style Preferences applicable to drafting views.
|
SpecifySectionLineBuilder |
Select a section line .
|
StandardViewsBuilder |
This builder allows the user to create a Drawing View
To create a new instance of this class, use DraftingViewCollection.createStandardViewsBuilder() Default values. |
SteppedSectionLine |
A Simple or Stepped Section Line.
|
SteppedSectionLineBuilder | Deprecated
Deprecated in NX10.0.0.
|
SvtBuilder | |
ThreadsViewStyle |
Represents set of Threads View Style Preferences applicable to drafting views.
|
TraceLinesViewStyle |
Represents interface for Trace Lines View Style Preferences applicable to drafting views.
|
TrackDrawingChangesGeneralBuilder | |
TrackDrawingChangesReportFilterBuilder |
Represents a
Drawings.TrackDrawingChangesReportFilterBuilder
Created in NX11.0.0 |
UpdateViewsBuilder |
Represents a
UpdateViewsBuilder
To create a new instance of this class, use DraftingViewCollection.createUpdateViewsBuilder() Created in NX5.0.0 |
View2dOrientBuilder |
Represents the View 2D Orientation (Drawings.View2dOrientBuilder)
Created in NX6.0.0 |
ViewAlignment |
View Alignment object.
|
ViewAlignmentBuilder |
Represents a
ViewAlignmentBuilder .This class is used to construct the view alignment Builder To create a new instance of this class, use ViewAlignmentCollection.createViewAlignmentBuilder() Default values. |
ViewAlignmentCollection |
Represents a collection of
ViewAlignment s. |
ViewBoundaryBuilder |
Represents the View Boundary (Drawings.ViewBoundaryBuilder)
Created in NX6.0.0 |
ViewBreak |
ViewBreak - defines the portion of a view that gets hidden to
produce a broken view
To create or edit an instance of this class, use BrokenViewBuilder Created in NX7.5.0 |
ViewBreakBuilder |
Represents a
ViewBreakBuilder This is a sub-builder class and cannot be directly instantiated Created in NX9.0.0 |
ViewBreakCollection |
Represents a collection of
ViewBreak s. |
ViewCenterCoordinateBuilder |
Represents the View center coodinate (Drawings.ViewCenterCoordinateBuilder)
Created in NX6.0.0 |
ViewCommonViewLabelBuilder | |
ViewCopyTo3dBuilder |
Represents a
ViewCopyTo3dBuilder . |
ViewCreationWizardBuilder |
This builder allows the user to create a Drawing View
To create a new instance of this class, use DraftingViewCollection.createViewCreationWizardBuilder() Default values. |
ViewDetailLabelBuilder | |
ViewingDirectionArrow |
This class represents a Drafting Viewing Direction Arrow.
|
ViewingDirectionArrowLabel |
This class represents a Drafting Viewing Direction Arrow Label.
|
ViewLabelBuilder | |
ViewOrientationBuilder |
Represents a ViewOrientationBuilder.
|
ViewPlacementBuilder |
Represents a
ViewPlacementBuilder . |
ViewProjectedArrowSettingsBuilder | |
ViewProjectedLabelBuilder | |
ViewProjectedViewSettingsBuilder | |
ViewProjectionBuilder |
Represents a
ViewProjectionBuilder . |
ViewProjectionPlaneBuilder |
Represents the View Projection Plane (Drawings.ViewProjectionPlaneBuilder)
Created in NX6.0.2 |
ViewScaleBuilder |
Represents the View Scale (Drawings.ViewScaleBuilder)
Created in NX6.0.0 |
ViewSectionLabelBuilder | |
ViewSectionLineBuilder | |
ViewSettingsBuilder |
Represents a
Drawings.ViewSettingsBuilder . |
ViewStyle |
Represents set of style applicable to drafting views.
|
ViewStyleBaseBuilder |
Represents the BASE tab on the View Style Dialog (Drawings.ViewStyleBaseBuilder)
Created in NX6.0.0 |
ViewStyleBuilder |
Represents the View Style Builder (Drawings.ViewStyleBuilder) which manages all the style attributes related
to the view including base view, projected view, drawing view, detail view, broken view, section view etc.
|
ViewStyleDetailBuilder |
Represents the DETAIL tab on the View Style Dialog (Drawings.ViewStyleDetailBuilder)
Created in NX6.0.0 |
ViewStyleFPCalloutConfigBuilder |
Represents the Callout section of the Flat Pattern tab on the View Style Dialog (Drawings.ViewStyleFPCalloutsBuilder)
Created in NX9.0.0 |
ViewStyleFPCalloutsBuilder |
Represents the Callout section of the Flat Pattern tab on the View Style Dialog (Drawings.ViewStyleFPCalloutsBuilder)
Created in NX6.0.0 |
ViewStyleFPCurvesBuilder |
Represents the Curve section of the Flat Pattern tab on the View Style Dialog (Drawings.ViewStyleFPCurvesBuilder)
Created in NX6.0.0 |
ViewStyleGeneralBuilder |
Represents view style general builder (Drawings.ViewStyleGeneralBuilder) which manages all the general
attributes which are necessary for all the views.
|
ViewStyleHiddenLinesBuilder |
Represents the HIDDEN LINES tab on the View Style Dialog (Drawings.ViewStyleHiddenLinesBuilder)
Created in NX6.0.0 |
ViewStyleInheritPmiBuilder |
Represents the INHERIT PMI tab on the View Style Dialog (Drawings.ViewStyleInheritPmiBuilder)
Created in NX6.0.0 |
ViewStyleOrientationBuilder |
Represents the ORIENTATION tab on the View Style Dialog (Drawings.ViewStyleOrientationBuilder)
Created in NX6.0.0 |
ViewStylePerspectiveBuilder |
Represents the PERSPECTIVE tab on the View Style Dialog (Drawings.ViewStylePerspectiveBuilder)
Created in NX6.0.0 |
ViewStyleProjectedBuilder |
Represents the PROJECTED tab on the View Style Dialog (Drawings.ViewStyleProjectedBuilder)
Created in NX6.0.0 |
ViewStyleSecondaryComponentsBuilder |
Represents the Secondary Geometry tab on the View Style Dialog (Drawings.ViewStyleHiddenLinesBuilder)
Created in NX11.0.0 |
ViewStyleSectionBuilder |
Represents the SECTION tab on the View Style Dialog (Drawings.ViewStyleSectionBuilder)
Created in NX6.0.0 |
ViewStyleSectionConstraintsBuilder |
Represents the SECTION CONSTRAINTS tab on the View Style Dialog (Drawings.ViewStyleSectionConstraintsBuilder)
Created in NX6.0.0 |
ViewStyleShadingBuilder |
Represents the SHADING tab on the View Style Dialog (Drawings.ViewStyleShadingBuilder)
Created in NX6.0.0 |
ViewStyleShipbuildingLinesBuilder |
Represents the Shipbuilding LINES tab on the View Style Dialog (Drawings.ViewStyleShipbuildingLinesBuilder)
To create a new instance of this class, use DraftingViewCollection.createShipbuildingLineBuilder() Created in NX8.0.0 |
ViewStyleShipbuildingLinesBuilderList |
Represents a list of objects.
|
ViewStyleSmoothEdgesBuilder |
Represents the SMOOTH EDGES tab on the View Style Dialog (Drawings.ViewStyleSmoothEdgesBuilder)
Created in NX6.0.0 |
ViewStyleThreadsBuilder |
Represents the THREADS tab on the View Style Dialog (Drawings.ViewStyleThreadsBuilder)
Created in NX6.0.0 |
ViewStyleTraceLinesBuilder |
Represents the TRACE LINES tab on the View Style Dialog (Drawings.ViewStyleTraceLinesBuilder)
Created in NX6.0.0 |
ViewStyleVirtualIntersectionsBuilder |
Represents the VIRTUAL INTERSECTIONS tab on the View Style Dialog (Drawings.ViewStyleVirtualIntersectionsBuilder)
Created in NX6.0.0 |
ViewStyleVisibleLinesBuilder |
Represents the VISIBLE LINES tab on the View Style Dialog (Drawings.ViewStyleVisibleLinesBuilder)
Created in NX6.0.0 |
ViewWorkflowBuilder | |
VirtualIntersectionsViewStyle |
Represents set of Virtual Intersections View Style Preferences applicable to drafting views.
|
VisibleAndHiddenLinesColorFontWidthBuilder |
Represent a
VisibleAndHiddenLinesColorFontWidthBuilder
This is a sub-builder class and cannot be directly instantiated Created in NX11.0.0 |
VisibleLinesViewStyle |
Represents set of Visible Lines View Style Preferences applicable to drafting views.
|
VisualDrawingComparePrefsBuilder |
This class gets and sets components of Visual Overlay in Drafting Preferences.
|
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.