public static class AnnotationSettingsBuilder.AnnotationTypeEnum extends Enum
Modifier and Type | Method and Description |
---|---|
static AnnotationSettingsBuilder.AnnotationTypeEnum |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AnnotationSettingsBuilder.AnnotationTypeEnum |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AnnotationSettingsBuilder.AnnotationTypeEnum[] |
values()
Returns an array that contains the values for this enum.
|
public static final AnnotationSettingsBuilder.AnnotationTypeEnum DIMENSION
public static final AnnotationSettingsBuilder.AnnotationTypeEnum NOTE
public static final AnnotationSettingsBuilder.AnnotationTypeEnum FEATURE_CONTROL_FRAME
public static final AnnotationSettingsBuilder.AnnotationTypeEnum DATUM_FEATURE_SYMBOL
public static final AnnotationSettingsBuilder.AnnotationTypeEnum DATUM_TARGET
public static final AnnotationSettingsBuilder.AnnotationTypeEnum BALLOON
public static final AnnotationSettingsBuilder.AnnotationTypeEnum SURFACE_FINISH_SYMBOL
public static final AnnotationSettingsBuilder.AnnotationTypeEnum WELD_SYMBOL
public static final AnnotationSettingsBuilder.AnnotationTypeEnum CUSTOM_SYMBOL
public static final AnnotationSettingsBuilder.AnnotationTypeEnum CENTER_LINE
public static final AnnotationSettingsBuilder.AnnotationTypeEnum USER_DEFINED_SYMBOL
public static final AnnotationSettingsBuilder.AnnotationTypeEnum MAX_ANNOTATION_YYPES
public static final int _DIMENSION
public static final int _NOTE
public static final int _FEATURE_CONTROL_FRAME
public static final int _DATUM_FEATURE_SYMBOL
public static final int _DATUM_TARGET
public static final int _BALLOON
public static final int _SURFACE_FINISH_SYMBOL
public static final int _WELD_SYMBOL
public static final int _CUSTOM_SYMBOL
public static final int _CENTER_LINE
public static final int _USER_DEFINED_SYMBOL
public static final int _MAX_ANNOTATION_YYPES
public static AnnotationSettingsBuilder.AnnotationTypeEnum valueOf(int value)
public static AnnotationSettingsBuilder.AnnotationTypeEnum valueOf(String name)
public static AnnotationSettingsBuilder.AnnotationTypeEnum[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.