public static class HingeLineBuilder.Hingeline extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DEFINED
The option for selecting hinge line using vector construction tools
|
static int |
_INFERRED
The option to infer a hinge line based on parent, child view position
|
static HingeLineBuilder.Hingeline |
DEFINED
The option for selecting hinge line using vector construction tools
|
static HingeLineBuilder.Hingeline |
INFERRED
The option to infer a hinge line based on parent, child view position
|
Modifier and Type | Method and Description |
---|---|
static HingeLineBuilder.Hingeline |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HingeLineBuilder.Hingeline |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HingeLineBuilder.Hingeline[] |
values()
Returns an array that contains the values for this enum.
|
public static final HingeLineBuilder.Hingeline INFERRED
public static final HingeLineBuilder.Hingeline DEFINED
public static final int _INFERRED
public static final int _DEFINED
public static HingeLineBuilder.Hingeline valueOf(int value)
public static HingeLineBuilder.Hingeline valueOf(String name)
public static HingeLineBuilder.Hingeline[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.