public static class DrawingsPropertiesBuilder.SecondaryComponentOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MIXED
Objects secondary geometry properties differ and will not change
|
static int |
_NO
Not marked as secondary geometry
|
static int |
_YES
Marked as secondary geometry
|
static DrawingsPropertiesBuilder.SecondaryComponentOptions |
MIXED
Objects secondary geometry properties differ and will not change
|
static DrawingsPropertiesBuilder.SecondaryComponentOptions |
NO
Not marked as secondary geometry
|
static DrawingsPropertiesBuilder.SecondaryComponentOptions |
YES
Marked as secondary geometry
|
Modifier and Type | Method and Description |
---|---|
static DrawingsPropertiesBuilder.SecondaryComponentOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrawingsPropertiesBuilder.SecondaryComponentOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrawingsPropertiesBuilder.SecondaryComponentOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final DrawingsPropertiesBuilder.SecondaryComponentOptions NO
public static final DrawingsPropertiesBuilder.SecondaryComponentOptions YES
public static final DrawingsPropertiesBuilder.SecondaryComponentOptions MIXED
public static final int _NO
public static final int _YES
public static final int _MIXED
public static DrawingsPropertiesBuilder.SecondaryComponentOptions valueOf(int value)
public static DrawingsPropertiesBuilder.SecondaryComponentOptions valueOf(String name)
public static DrawingsPropertiesBuilder.SecondaryComponentOptions[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.