public static class ViewProjectionBuilder.Types extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_PROJECT_ON_ONE_PLANE
on one plane
|
static int |
_PROJECT_ON_TWO_PLANES
on two planes
|
static ViewProjectionBuilder.Types |
PROJECT_ON_ONE_PLANE
on one plane
|
static ViewProjectionBuilder.Types |
PROJECT_ON_TWO_PLANES
on two planes
|
Modifier and Type | Method and Description |
---|---|
static ViewProjectionBuilder.Types |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ViewProjectionBuilder.Types |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ViewProjectionBuilder.Types[] |
values()
Returns an array that contains the values for this enum.
|
public static final ViewProjectionBuilder.Types PROJECT_ON_ONE_PLANE
public static final ViewProjectionBuilder.Types PROJECT_ON_TWO_PLANES
public static final int _PROJECT_ON_ONE_PLANE
public static final int _PROJECT_ON_TWO_PLANES
public static ViewProjectionBuilder.Types valueOf(int value)
public static ViewProjectionBuilder.Types valueOf(String name)
public static ViewProjectionBuilder.Types[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.