public static class GeneralWorkFlowBuilder.ModelBasedAlwaysStartType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BASE_VIEW_COMMAND |
static int |
_NO_VIEW_COMMANDS |
static int |
_VIEW_CREATION_WIZARD |
static GeneralWorkFlowBuilder.ModelBasedAlwaysStartType |
BASE_VIEW_COMMAND |
static GeneralWorkFlowBuilder.ModelBasedAlwaysStartType |
NO_VIEW_COMMANDS |
static GeneralWorkFlowBuilder.ModelBasedAlwaysStartType |
VIEW_CREATION_WIZARD |
Modifier and Type | Method and Description |
---|---|
static GeneralWorkFlowBuilder.ModelBasedAlwaysStartType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GeneralWorkFlowBuilder.ModelBasedAlwaysStartType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GeneralWorkFlowBuilder.ModelBasedAlwaysStartType[] |
values()
Returns an array that contains the values for this enum.
|
public static final GeneralWorkFlowBuilder.ModelBasedAlwaysStartType VIEW_CREATION_WIZARD
public static final GeneralWorkFlowBuilder.ModelBasedAlwaysStartType BASE_VIEW_COMMAND
public static final GeneralWorkFlowBuilder.ModelBasedAlwaysStartType NO_VIEW_COMMANDS
public static final int _VIEW_CREATION_WIZARD
public static final int _BASE_VIEW_COMMAND
public static final int _NO_VIEW_COMMANDS
public static GeneralWorkFlowBuilder.ModelBasedAlwaysStartType valueOf(int value)
public static GeneralWorkFlowBuilder.ModelBasedAlwaysStartType valueOf(String name)
public static GeneralWorkFlowBuilder.ModelBasedAlwaysStartType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.