public interface PointAndAngleSectionLineBuilder extends TaggedObject, IComponentBuilder
PointAndAngleSectionLineBuilder
.
This class is used to create or edit a
PointAndAngleSectionLine
.
Modifier and Type | Method and Description |
---|---|
Point |
endLocation1()
Deprecated.
Deprecated in NX10.0.0. This API is not supported yet and should not be used.
|
Point |
endLocation2()
Deprecated.
Deprecated in NX10.0.0. This API is not supported yet and should not be used.
|
SectionLineSegmentBuilderList |
leg1()
Deprecated.
Deprecated in NX10.0.0. This API is not supported yet and should not be used.
|
void |
setEndLocation1(Point endLocation1)
Deprecated.
Deprecated in NX10.0.0. This API is not supported yet and should not be used.
|
void |
setEndLocation2(Point endLocation2)
Deprecated.
Deprecated in NX10.0.0. This API is not supported yet and should not be used.
|
printTestData, printTestData, tag, tagValue
validate
SectionLineSegmentBuilderList leg1() throws NXException, RemoteException
SectionLineSegmentBuilder
segments of type SectionLineSegmentBuilder.Types.ANGLE
only.
Note that the segments are added in the order that they appear in this list.
NXException
RemoteException
Point endLocation1() throws NXException, RemoteException
NXException
RemoteException
void setEndLocation1(Point endLocation1) throws NXException, RemoteException
endLocation1
- NXException
RemoteException
Point endLocation2() throws NXException, RemoteException
NXException
RemoteException
void setEndLocation2(Point endLocation2) throws NXException, RemoteException
endLocation2
- NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.