public static class DrawingCompareSettingsBuilder.WidthType extends Enum
Modifier and Type | Method and Description |
---|---|
static DrawingCompareSettingsBuilder.WidthType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrawingCompareSettingsBuilder.WidthType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrawingCompareSettingsBuilder.WidthType[] |
values()
Returns an array that contains the values for this enum.
|
public static final DrawingCompareSettingsBuilder.WidthType THIN
public static final DrawingCompareSettingsBuilder.WidthType NORMAL
public static final DrawingCompareSettingsBuilder.WidthType THICK
public static final DrawingCompareSettingsBuilder.WidthType ONE
public static final DrawingCompareSettingsBuilder.WidthType TWO
public static final DrawingCompareSettingsBuilder.WidthType THREE
public static final DrawingCompareSettingsBuilder.WidthType FOUR
public static final DrawingCompareSettingsBuilder.WidthType FIVE
public static final DrawingCompareSettingsBuilder.WidthType SIX
public static final DrawingCompareSettingsBuilder.WidthType SEVEN
public static final DrawingCompareSettingsBuilder.WidthType EIGHT
public static final DrawingCompareSettingsBuilder.WidthType NINE
public static final int _THIN
public static final int _NORMAL
public static final int _THICK
public static final int _ONE
public static final int _TWO
public static final int _THREE
public static final int _FOUR
public static final int _FIVE
public static final int _SIX
public static final int _SEVEN
public static final int _EIGHT
public static final int _NINE
public static DrawingCompareSettingsBuilder.WidthType valueOf(int value)
public static DrawingCompareSettingsBuilder.WidthType valueOf(String name)
public static DrawingCompareSettingsBuilder.WidthType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.