public static class TrackDrawingChangesGeneralBuilder.CompareMethodType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AGAINST_ANOTHER_DRAWING
This option is used to compare different part over current part
|
static int |
_AGAINST_SNAPSHOT_DATA_IN_ACTIVE_DRAWING
This option is used to compare current part on itself
|
static int |
_OPEN_SAVED_COMPARISON_REPORT
This option is used to open a compare report that is saved in the current part
|
static TrackDrawingChangesGeneralBuilder.CompareMethodType |
AGAINST_ANOTHER_DRAWING
This option is used to compare different part over current part
|
static TrackDrawingChangesGeneralBuilder.CompareMethodType |
AGAINST_SNAPSHOT_DATA_IN_ACTIVE_DRAWING
This option is used to compare current part on itself
|
static TrackDrawingChangesGeneralBuilder.CompareMethodType |
OPEN_SAVED_COMPARISON_REPORT
This option is used to open a compare report that is saved in the current part
|
Modifier and Type | Method and Description |
---|---|
static TrackDrawingChangesGeneralBuilder.CompareMethodType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrackDrawingChangesGeneralBuilder.CompareMethodType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrackDrawingChangesGeneralBuilder.CompareMethodType[] |
values()
Returns an array that contains the values for this enum.
|
public static final TrackDrawingChangesGeneralBuilder.CompareMethodType AGAINST_ANOTHER_DRAWING
public static final TrackDrawingChangesGeneralBuilder.CompareMethodType AGAINST_SNAPSHOT_DATA_IN_ACTIVE_DRAWING
public static final TrackDrawingChangesGeneralBuilder.CompareMethodType OPEN_SAVED_COMPARISON_REPORT
public static final int _AGAINST_ANOTHER_DRAWING
public static final int _AGAINST_SNAPSHOT_DATA_IN_ACTIVE_DRAWING
public static final int _OPEN_SAVED_COMPARISON_REPORT
public static TrackDrawingChangesGeneralBuilder.CompareMethodType valueOf(int value)
public static TrackDrawingChangesGeneralBuilder.CompareMethodType valueOf(String name)
public static TrackDrawingChangesGeneralBuilder.CompareMethodType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.