public static class CustomViewSettingsBuilder.Features extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_HIDE |
static int |
_SHOW_ALL |
static int |
_SIMPLIFY |
static CustomViewSettingsBuilder.Features |
HIDE |
static CustomViewSettingsBuilder.Features |
SHOW_ALL |
static CustomViewSettingsBuilder.Features |
SIMPLIFY |
Modifier and Type | Method and Description |
---|---|
static CustomViewSettingsBuilder.Features |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CustomViewSettingsBuilder.Features |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CustomViewSettingsBuilder.Features[] |
values()
Returns an array that contains the values for this enum.
|
public static final CustomViewSettingsBuilder.Features SHOW_ALL
public static final CustomViewSettingsBuilder.Features SIMPLIFY
public static final CustomViewSettingsBuilder.Features HIDE
public static final int _SHOW_ALL
public static final int _SIMPLIFY
public static final int _HIDE
public static CustomViewSettingsBuilder.Features valueOf(int value)
public static CustomViewSettingsBuilder.Features valueOf(String name)
public static CustomViewSettingsBuilder.Features[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.