public static class DrawingSheet.StandardSheetSize extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_A
8.5 x 11 inches
|
static int |
_A0
841 x 1189 millimeters
|
static int |
_A1
594 X 841 millimeters
|
static int |
_A2
420 X 594 millimeters
|
static int |
_A3
297 X 420 millimeters
|
static int |
_A4
210 X 297 millimeters
|
static int |
_B
11 X 17 inches
|
static int |
_C
17 X 22 inches
|
static int |
_D
22 X 34 inches
|
static int |
_E
34 X 44 inches
|
static int |
_F
28 X 40 inches
|
static int |
_H
28 X 44 inches
|
static int |
_J
34 X 55 inches
|
static DrawingSheet.StandardSheetSize |
A
8.5 x 11 inches
|
static DrawingSheet.StandardSheetSize |
A0
841 x 1189 millimeters
|
static DrawingSheet.StandardSheetSize |
A1
594 X 841 millimeters
|
static DrawingSheet.StandardSheetSize |
A2
420 X 594 millimeters
|
static DrawingSheet.StandardSheetSize |
A3
297 X 420 millimeters
|
static DrawingSheet.StandardSheetSize |
A4
210 X 297 millimeters
|
static DrawingSheet.StandardSheetSize |
B
11 X 17 inches
|
static DrawingSheet.StandardSheetSize |
C
17 X 22 inches
|
static DrawingSheet.StandardSheetSize |
D
22 X 34 inches
|
static DrawingSheet.StandardSheetSize |
E
34 X 44 inches
|
static DrawingSheet.StandardSheetSize |
F
28 X 40 inches
|
static DrawingSheet.StandardSheetSize |
H
28 X 44 inches
|
static DrawingSheet.StandardSheetSize |
J
34 X 55 inches
|
Modifier and Type | Method and Description |
---|---|
static DrawingSheet.StandardSheetSize |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrawingSheet.StandardSheetSize |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrawingSheet.StandardSheetSize[] |
values()
Returns an array that contains the values for this enum.
|
public static final DrawingSheet.StandardSheetSize A
public static final DrawingSheet.StandardSheetSize B
public static final DrawingSheet.StandardSheetSize C
public static final DrawingSheet.StandardSheetSize D
public static final DrawingSheet.StandardSheetSize E
public static final DrawingSheet.StandardSheetSize F
public static final DrawingSheet.StandardSheetSize H
public static final DrawingSheet.StandardSheetSize J
public static final DrawingSheet.StandardSheetSize A0
public static final DrawingSheet.StandardSheetSize A1
public static final DrawingSheet.StandardSheetSize A2
public static final DrawingSheet.StandardSheetSize A3
public static final DrawingSheet.StandardSheetSize A4
public static final int _A
public static final int _B
public static final int _C
public static final int _D
public static final int _E
public static final int _F
public static final int _H
public static final int _J
public static final int _A0
public static final int _A1
public static final int _A2
public static final int _A3
public static final int _A4
public static DrawingSheet.StandardSheetSize valueOf(int value)
public static DrawingSheet.StandardSheetSize valueOf(String name)
public static DrawingSheet.StandardSheetSize[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.