public interface BaseViewStyle extends IBaseViewPreferences
Drawings.ViewStyle#baseView
Modifier and Type | Method and Description |
---|---|
void |
loadModelFromPart(String loadPartName,
boolean loadPartToggle)
To load the assemblies arrangement part file.
|
void |
setAssemblyArrangement(String config)
Sets the configuration for the arrangement in assembly after an
arrangement part file is loaded.
|
void |
setFacetedRepresentation(boolean isFacetedRepresentation)
Deprecated.
Deprecated in NX8.5.1. Use
Drawings.GeneralViewStyle#setViewRepresentation instead.
|
void |
setInheritClippingBoundary(boolean isInheritClippingBoundary)
The status of inherit clipping boundary, if True the model view's
clipping boundary are inherited when model view is imported onto the drawing, else
the imported model view is placed on the drawing with an Automatic Rectangular Boundary.
|
void |
setTransferAnnotation(boolean isTransferAnnotation)
The status of transfer annotation controls whether or not annotations created in
a model view are transferred to the drawing when a view is imported.
|
void setFacetedRepresentation(boolean isFacetedRepresentation) throws NXException, RemoteException
Drawings.GeneralViewStyle#setViewRepresentation
instead.
isFacetedRepresentation
- NXException
RemoteException
void setInheritClippingBoundary(boolean isInheritClippingBoundary) throws NXException, RemoteException
isInheritClippingBoundary
- Inherit XY clipping boundaries of modelNXException
RemoteException
void setTransferAnnotation(boolean isTransferAnnotation) throws NXException, RemoteException
isTransferAnnotation
- NXException
RemoteException
void setAssemblyArrangement(String config) throws NXException, RemoteException
config
- name of the configuration for the arrangementNXException
RemoteException
void loadModelFromPart(String loadPartName, boolean loadPartToggle) throws NXException, RemoteException
loadPartName
- name of the loaded partloadPartToggle
- True or False status for loading the part.NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.