AeroFlangeBuilderCompType Enumeration |
This method defines the types of Flange Compensation |
AeroFlangeBuilderDimType Enumeration |
This enum defines the flange length dimension types |
AeroFlangeBuilderDirType Enumeration |
This enum defines the type of direction vector |
AeroFlangeBuilderEndType Enumeration |
This enum defines the ends of a bend edge |
AeroFlangeBuilderLengthType Enumeration |
This enum defines the length type options. |
AeroFlangeBuilderMatType Enumeration |
This enum defines the material types |
AeroJoggleBuilderSideType Enumeration |
This enum defines the side of a twin joggle only side1 is used for a single joggle |
AeroLighteningCutoutBuilderTypes Enumeration |
Represents the cutout type. |
ApplicationContext Enumeration |
This is the enum representing application context of the feature |
BeadBuilderCrossSectionTypeOptions Enumeration |
This enum represents the cross section type options for the Bead. |
BeadBuilderEndTypeOptions Enumeration |
This enum represents the end type options for the Bead. |
BeadBuilderHeightSideOptions Enumeration |
This enum represents the depth direction for the Bead. |
BendBuilderBendDirectionOptions Enumeration |
This enum represents the Bend Direction for Bend. |
BendBuilderBendLocationOptions Enumeration |
This enum represents the Bend Location (Material Side) for Bend. |
BendBuilderFixedSideOptions Enumeration |
This enum represents the Fixed Side for Bend. |
BendOptionsBendReliefTypeOptions Enumeration |
This enum represents the bend relief type. |
BendOptionsCornerReliefTypeOptions Enumeration |
This enum represents the corner relief type. |
BendTaperBuilderBendTaperInputMethod Enumeration |
This enum represents the input methods for the bend taper. |
BendTaperBuilderBendTaperSides Enumeration |
This enum represents the taper sides options for the bend taper. |
BendTaperBuilderBendTaperType Enumeration |
This enum represents the bend taper types for the bend taper. |
BendTaperBuilderChainingType Enumeration |
This enum represents the chaining options for the bend taper. |
BendTaperBuilderStartType Enumeration |
This enum represents the start types for the bend taper. |
BendTaperBuilderWebTaperType Enumeration |
This enum represents the web taper types for the bend taper. |
BreakCornerBuilderTypeOptions Enumeration |
This enum represents the break corner type. |
BridgeTransitionBuilderInsetOptions Enumeration |
Enum representing the side of the Bridge Transition material with respect to the specified tangent plane. |
BridgeTransitionBuilderTypeOptions Enumeration |
Enum representing types for Bridge Transition feature. |
BridgeTransitionBuilderWidthDirectionOptions Enumeration |
Enum representing the width direction for the Bridge Transition. |
BridgeTransitionBuilderWidthOptions Enumeration |
Enum representing width option types for Bridge Transition feature. |
ClosedCornerBuilderClosureTypeOptions Enumeration |
This enum represents Corner Closure type |
ClosedCornerBuilderOriginTypes Enumeration |
This enum represents Origin type |
ClosedCornerBuilderTreatmentTypeOptions Enumeration |
This enum represents Corner treatment type |
ClosedCornerBuilderTypes Enumeration |
This enum represents the feature types. |
ContourFlangeBuilderSectionSideOptions Enumeration |
This enum represents the side of the section in which material is created. |
ContourFlangeBuilderSweepSideOptions Enumeration |
This enum represents the side in which the contour flange will be swept. |
ContourFlangeBuilderSweepTypeOptions Enumeration |
This enum represents the sweep type of the contour flange |
ConvertToSheetmetalBuilderBendReliefTypeOptions Enumeration |
This enum represents the bend relief type. |
CornerTreatmentBuilderCornerTreatmentType Enumeration |
Corner Treatment Type |
DimpleBuilderDepthTypeOptions Enumeration |
This enum represents the depth direction for the dimple. |
DimpleBuilderDimensionTypeOptions Enumeration |
the Dimension options for dimple. |
DimpleBuilderSectionSideOptions Enumeration |
This enum represents the side of the section that the dimple punches material. |
DimpleBuilderSidewallTypeOptions Enumeration |
the side walls material option. |
DrawnCutoutBuilderDepthTypeOptions Enumeration |
This enum represents the depth direction for the drawn cutout. |
DrawnCutoutBuilderSectionSideOptions Enumeration |
This enum represents the side of the section that the drawn cutout punches material. |
DrawnCutoutBuilderSidewallTypeOptions Enumeration |
The side walls material option. |
EditCornerBuilderBendClosureTypeOptions Enumeration |
This enum specifies the type of bend closure required at the corner. |
EditCornerBuilderCornerReliefTypeOptions Enumeration |
This enum specifies the type of relief required at the corner. |
EditCornerBuilderPlateClosureTypeOptions Enumeration |
This enum specifies the type of plate closure required at the corner. |
ExportFlatPatternBuilderDxfRevisionType Enumeration |
Specifies the DXF Revisions for flat pattern export |
ExportFlatPatternBuilderFileType Enumeration |
Specifies the flat pattern export type |
FeatureProperty Enumeration |
This is a common enum that comprises of values to be used for various features. |
FlangeBuilderInsetTypeOptions Enumeration |
This enum represents the inset type for the material of the flange. |
FlangeBuilderLengthTypeOptions Enumeration |
This enum indicates the two ways that the flange length can be measured. |
FlangeBuilderMatchFaceOptions Enumeration |
This enum represents the match face option for the flange. |
FlangeBuilderOffsetTypeOptions Enumeration |
This enum represents the offset type for the flange. |
FlangeBuilderWidthTypeOptions Enumeration |
This enum represents the width type for the flange. |
FlatSolidBuilderTransformComponentsOption Enumeration |
The enum defines how to represent PCB components on flat solid. |
FlexibleCableBuilderBendAngleDirectionOptions Enumeration |
This enum represents the bend angle direction for the bend segment. |
FlexibleCableBuilderPathAdjustmentAngleDirectionOptions Enumeration |
This enum represents the path adjustment angle direction for the bend segment. |
FlexibleCableBuilderSegmentTypeOptions Enumeration |
Represents the Flexible Cable segment options. |
GussetBuilderPlacementTypes Enumeration |
This enum represents the different options for placing an automatic profile Gusset. |
GussetBuilderShapes Enumeration |
This enum represents the two different shapes for Gusset. |
GussetBuilderTypes Enumeration |
This enum represents the two Gusset Feature types. |
GussetBuilderWidthSides Enumeration |
This enum represents the different options for thickening the user defined profile Gusset. |
HemFlangeBuilderBendReliefOptions Enumeration |
This enum represents the Bend relief type of the hem flange. |
HemFlangeBuilderInsetTypeOptions Enumeration |
This enum represents the inset type for the material of the hem flange. |
HemFlangeBuilderTypeOptions Enumeration |
Represents the Hem Flange type. |
JogBuilderBendLocationOptions Enumeration |
Represents the bend location type. |
JogBuilderDimensionTypeOptions Enumeration |
the Dimension options for jog. |
JogBuilderDirectionTypeOptions Enumeration |
this enum represents the direction for the Jog. |
JogBuilderFixedSideOptions Enumeration |
The left option represents the side to the left of a person who is walking along the section in the direction of its curves when the section normal is pointing up. |
LoftedFlangeBuilderSectionSideOptions Enumeration |
This enum represents the side of the section that the lofted flange creates thickness. |
LouverBuilderDepthSideOptions Enumeration |
This enum represents the depth side for the louver. |
LouverBuilderEndTypeOptions Enumeration |
This enum represents the end type for the louver. |
LouverBuilderSectionSideOptions Enumeration |
This enum represents the side of the section that the louver width is measured. |
MiterOptionsClosedCornerTypeOptions Enumeration |
the closed corner type options. |
MiterOptionsPositionOptions Enumeration |
the miter positions options. |
MiterOptionsTypeOptions Enumeration |
the miter type options. |
NormalCutoutBuilderCutTypeOptions Enumeration |
This enum represents the cut type for the normal cutout. |
NormalCutoutBuilderDepthSideOptions Enumeration |
This enum represents the depth direction for the normal cutout. |
NormalCutoutBuilderDepthTypeOptions Enumeration |
This enum represents the depth type for the normal cutout. |
NormalCutoutBuilderSectionSideOptions Enumeration |
This enum represents the side of the section that the normal cutout removes material. |
NormalCutoutBuilderTypeOptions Enumeration |
Represents the type of the normal cutout - sketch type OR 3D-curve type |
ResizeBendRadiusBuilderBendReliefTypeOptions Enumeration |
This enum represents the bend relief type. |
ResizeBendRadiusBuilderTypes Enumeration |
This enum represents the feature types. |
SMBoundaryConditionBuilderConstraintTypes Enumeration |
Types of Boundary condition constraints |
SheetmetalBendState Enumeration |
Bend State |
SheetmetalFaceLayer Enumeration |
Face Layer |
SheetmetalFaceType Enumeration |
Face Type |
SheetmetalManagerFlangeWidthOption Enumeration |
Flange width option |
SheetmetalManagerTabSweepDir Enumeration |
This enum is for Tab sweep direction flag. |
SheetmetalManagerTabType Enumeration |
This is the enum for Tab type i. |
SolidPunchBuilderTypes Enumeration |
Represents the punch type |
TabBuilderSectionSideOptions Enumeration |
This enum represents the side of the section that the dimple punches material. |
TabBuilderThicknessSideOptions Enumeration |
This enum represents the extent direction for the Tab. |
ThreeBendCornerBuilderOriginTypes Enumeration |
This enum represents Origin type |
ThreeBendCornerBuilderTreatmentTypeOptions Enumeration |
This enum represents the corner treatment type. |