ResizeBendAngleBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
ResizeBendAngleBuilder
¶ Bases:
NXOpen.Features.SheetMetal.SheetmetalBaseBuilder
Represents a
NXOpen.Features.ResizeBendAngle
builderTo create a new instance of this class, use
NXOpen.Features.SheetMetal.SheetmetalManager.CreateResizeBendAngleBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Angle | Returns the bend angle |
BendFace | Returns the bend face |
KeepRadiusFixed | Returns or sets the flag indicationg to keep radius fixed |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ReferenceEdge | Returns the reference edge |
ReferenceFace | Returns the reference face |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetApplicationContext | Get the application context. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetApplicationContext | Set the application context. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Angle¶
-
ResizeBendAngleBuilder.
Angle
¶ Returns the bend angle
-------------------------------------
Getter Method
Signature
Angle()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
BendFace¶
-
ResizeBendAngleBuilder.
BendFace
¶ Returns the bend face
-------------------------------------
Getter Method
Signature
BendFace()
Returns: Return type: NXOpen.SelectFace
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
KeepRadiusFixed¶
-
ResizeBendAngleBuilder.
KeepRadiusFixed
¶ Returns or sets the flag indicationg to keep radius fixed
-------------------------------------
Getter Method
Signature
KeepRadiusFixed()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepRadiusFixed(keepRadiusFixed)
Parameters: keepRadiusFixed (bool) – New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
ReferenceEdge¶
-
ResizeBendAngleBuilder.
ReferenceEdge
¶ Returns the reference edge
-------------------------------------
Getter Method
Signature
ReferenceEdge()
Returns: Return type: NXOpen.SelectEdge
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
ReferenceFace¶
-
ResizeBendAngleBuilder.
ReferenceFace
¶ Returns the reference face
-------------------------------------
Getter Method
Signature
ReferenceFace()
Returns: Return type: NXOpen.SelectFace
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Method Detail¶
Validate¶
-
ResizeBendAngleBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.