BridgeTransitionBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
BridgeTransitionBuilder
¶ Bases:
NXOpen.Features.SheetMetal.SheetmetalBaseBuilder
Represents a Bridge Transition builder
To create a new instance of this class, use
NXOpen.Features.SheetMetal.SheetmetalManager.CreateBridgeTransitionBuilder
New in version NX5.0.2.
Properties¶
Property | Description |
---|---|
EndEdge | Returns the end edge |
EndRadius | Returns the inner bend radius of bend region near end edge. |
InsetType | Returns or sets the inset type |
Length | Returns the length of the planar region near start edge. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Plane | Returns the tangential plane |
Point | Returns or sets the point with respect to which the finite or symmetric width is specified. |
StartEdge | Returns the start edge |
StartRadius | Returns the inner bend radius of the bend region near start edge. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Type | Returns or sets the transition type |
Width | Returns the width |
WidthDirection | Returns or sets the width direction. |
WidthType | Returns or sets the width type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetApplicationContext | Get the application context. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetApplicationContext | Set the application context. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BridgeTransitionBuilderInsetOptions Enumeration | Enum representing the side of the Bridge Transition material with respect to the specified tangent plane. |
BridgeTransitionBuilderTypeOptions Enumeration | Enum representing types for Bridge Transition feature. |
BridgeTransitionBuilderWidthDirectionOptions Enumeration | Enum representing the width direction for the Bridge Transition. |
BridgeTransitionBuilderWidthOptions Enumeration | Enum representing width option types for Bridge Transition feature. |
Property Detail¶
EndEdge¶
-
BridgeTransitionBuilder.
EndEdge
¶ Returns the end edge
-------------------------------------
Getter Method
Signature
EndEdge()
Returns: Return type: NXOpen.SelectEdge
New in version NX5.0.2.
License requirements: nx_flexible_pcb (“NX Flexible PCB”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
EndRadius¶
-
BridgeTransitionBuilder.
EndRadius
¶ Returns the inner bend radius of bend region near end edge.
End radius required to be specified for
Features.SheetMetal.BridgeTransitionBuilderTypeOptions.Zu
.-------------------------------------
Getter Method
Signature
EndRadius()
Returns: Return type: NXOpen.Expression
New in version NX5.0.2.
License requirements: nx_flexible_pcb (“NX Flexible PCB”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
InsetType¶
-
BridgeTransitionBuilder.
InsetType
¶ Returns or sets the inset type
-------------------------------------
Getter Method
Signature
InsetType()
Returns: Return type: NXOpen.Features.SheetMetal.BridgeTransitionBuilderInsetOptions
New in version NX5.0.2.
License requirements: nx_flexible_pcb (“NX Flexible PCB”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
-------------------------------------
Setter Method
Signature
InsetType(insetType)
Parameters: insetType ( NXOpen.Features.SheetMetal.BridgeTransitionBuilderInsetOptions
) –New in version NX5.0.2.
License requirements: nx_flexible_pcb (“NX Flexible PCB”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
Length¶
-
BridgeTransitionBuilder.
Length
¶ Returns the length of the planar region near start edge.
Length is required to be specified for
Features.SheetMetal.BridgeTransitionBuilderTypeOptions.Fold
.-------------------------------------
Getter Method
Signature
Length()
Returns: Return type: NXOpen.Expression
New in version NX5.0.2.
License requirements: nx_flexible_pcb (“NX Flexible PCB”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
Plane¶
-
BridgeTransitionBuilder.
Plane
¶ Returns the tangential plane
-------------------------------------
Getter Method
Signature
Plane()
Returns: Return type: NXOpen.SelectISurface
New in version NX5.0.2.
License requirements: nx_flexible_pcb (“NX Flexible PCB”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
Point¶
-
BridgeTransitionBuilder.
Point
¶ Returns or sets the point with respect to which the finite or symmetric width is specified.
-------------------------------------
Getter Method
Signature
Point()
Returns: Return type: NXOpen.Point
New in version NX5.0.2.
License requirements: nx_flexible_pcb (“NX Flexible PCB”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
-------------------------------------
Setter Method
Signature
Point(point)
Parameters: point ( NXOpen.Point
) –New in version NX5.0.2.
License requirements: nx_flexible_pcb (“NX Flexible PCB”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
StartEdge¶
-
BridgeTransitionBuilder.
StartEdge
¶ Returns the start edge
-------------------------------------
Getter Method
Signature
StartEdge()
Returns: Return type: NXOpen.SelectEdge
New in version NX5.0.2.
License requirements: nx_flexible_pcb (“NX Flexible PCB”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
StartRadius¶
-
BridgeTransitionBuilder.
StartRadius
¶ Returns the inner bend radius of the bend region near start edge.
Start radius required to be specified for
Features.SheetMetal.BridgeTransitionBuilderTypeOptions.Zu
.-------------------------------------
Getter Method
Signature
StartRadius()
Returns: Return type: NXOpen.Expression
New in version NX5.0.2.
License requirements: nx_flexible_pcb (“NX Flexible PCB”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
Type¶
-
BridgeTransitionBuilder.
Type
¶ Returns or sets the transition type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.SheetMetal.BridgeTransitionBuilderTypeOptions
New in version NX5.0.2.
License requirements: nx_flexible_pcb (“NX Flexible PCB”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.SheetMetal.BridgeTransitionBuilderTypeOptions
) –New in version NX5.0.2.
License requirements: nx_flexible_pcb (“NX Flexible PCB”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
Width¶
-
BridgeTransitionBuilder.
Width
¶ Returns the width
-------------------------------------
Getter Method
Signature
Width()
Returns: Return type: NXOpen.Expression
New in version NX5.0.2.
License requirements: nx_flexible_pcb (“NX Flexible PCB”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
WidthDirection¶
-
BridgeTransitionBuilder.
WidthDirection
¶ Returns or sets the width direction.
Only applies if the width type is
Features.SheetMetal.BridgeTransitionBuilderWidthOptions.Finite
-------------------------------------
Getter Method
Signature
WidthDirection()
Returns: Return type: NXOpen.Features.SheetMetal.BridgeTransitionBuilderWidthDirectionOptions
New in version NX5.0.2.
License requirements: nx_flexible_pcb (“NX Flexible PCB”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
-------------------------------------
Setter Method
Signature
WidthDirection(widthDirection)
Parameters: widthDirection ( NXOpen.Features.SheetMetal.BridgeTransitionBuilderWidthDirectionOptions
) –New in version NX5.0.2.
License requirements: nx_flexible_pcb (“NX Flexible PCB”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
WidthType¶
-
BridgeTransitionBuilder.
WidthType
¶ Returns or sets the width type
-------------------------------------
Getter Method
Signature
WidthType()
Returns: Return type: NXOpen.Features.SheetMetal.BridgeTransitionBuilderWidthOptions
New in version NX5.0.2.
License requirements: nx_flexible_pcb (“NX Flexible PCB”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
-------------------------------------
Setter Method
Signature
WidthType(widthType)
Parameters: widthType ( NXOpen.Features.SheetMetal.BridgeTransitionBuilderWidthOptions
) –New in version NX5.0.2.
License requirements: nx_flexible_pcb (“NX Flexible PCB”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
Method Detail¶
Validate¶
-
BridgeTransitionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.